Part Number: MSP430FR5994
Hi,
I am attempting to initialize a pin (4.2) as an input pin tied low, but after configuration, it remains tied high. I am using the timer to periodically poll the value on the pin, and the value is always 4 (meaning BIT2 = 1) unless I tie that pin to ground using a jumper, in which case the value printed is 0.
Can anyone point out what is going wrong? My code is attached below.
#include <msp430.h>
#include <stdio.h>
//Global Variables
volatile int read = 0;
/**
* main.c
*/
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; //Stop WDT
//Configure Pins
P4OUT = 0;
P4DIR = ~BIT2; //Set 4.2 as Input
P4REN = BIT2; //Enable pulldown resistor 4.2
PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
// to activate previously configured port settings
//Set Timer A0
TA0CCTL0 = CCIE; // CCR0 interrupt enabled
TA0CTL = TASSEL__ACLK | MC_1; // Clock used is ACLK, Up mode (0 to TA0CCR0)
TA0CCR0 = 65535;
__enable_interrupt();
printf("TestProgram Start:\n");
while(1);
}
#pragma vector = TIMER0_A0_VECTOR;
__interrupt void Timer_A0 (void){
P1OUT ^= BIT0;
read = P4IN;
printf("Input: %d\n", read);
}
Thanks,
John