Other Parts Discussed in Thread: TPS2103, LM66100
I am currently working on an embedded design where the primary power source for the MSP430G2553 MCU is a CR2032 battery. The MCU is being used to power cycle another system. I was hoping to use the system to power the MCU via a 3V3 LDO (TLV70033) when it is switched on and then have the MCU powered from the battery when the system is powered off. I thought that the TPS2103 would work for this application, but I am having an issue where the MCU resets during the switch between the power supplies.
I have attached the current circuit here as well as the recommended circuit from the datasheet. The current debug code on the MCU simply turns an LED on, as this allows me to see if the MCU resets during the supply switch. I have experimented with multiple output capacitors to no avail. I used Figure 16 of the TPS2103 datasheet to select my capacitor values, but capacitors in the range of 1 uF to 220 uF seem to just force the MCU off when the supply switch happens. In the current configuration without an output capacitor, the MCU flickers on and off when the supply switch happens.
Is there a better component for what I am trying to do here? I think the issue is related to how sensitive the MCU is to a drop in the supply voltage, but I'm not 100% sure. Measuring the output of the TPS2103 using the Peak mode on my Fluke 87V shows a minimum of between 1.2 and 1.5 V when the switch happens. In the regular MaxMin mode, my meter reads a minimum of between 2.4 and 2.7 V (i.e. the voltage drop during the switch is very brief).
Current circuit:
Recommended circuit: