This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5437A: About Vcore connections

Part Number: MSP430F5437A


Hello,

I'd like to ask if the following connection of Vcore(MSP430F5437A pin#49) is correct. Please refer to the picture.

VCORE doesn't look like being connected correctly. The datasheet says as follows:

CVCORE : Recommended capacitor at VCORE 470nF.

All voltages referenced to VSS. VCORE is for internal device use only. No external DC loading or voltage should be applied.

Can you please check and give us an advice?

Thanks, HJ.

**Attention** This is a public forum