This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5529: Code Composer Studio™ forum

Part Number: MSP430F5529
Other Parts Discussed in Thread: ADS1100

Tool/software: Code Composer Studio

  
here is the initialization function call and the function

 TI_USCI_I2C_receiveinit(0x48,0x12);

void TI_USCI_I2C_receiveinit(unsigned char slave_address,
                             unsigned char prescale){

  P3SEL |= SDA_PIN + SCL_PIN;                 // Assign I2C pins to USCI_B0
  UCB0CTL1 = UCSWRST;                        // Enable SW reset
  UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;       // I2C Master, synchronous mode
  UCB0CTL1 = UCSSEL_2 + UCSWRST;              // Use SMCLK, keep SW reset
  UCB0BR0 = prescale;                         // set prescaler
  UCB0BR1 = 0;
  UCB0I2CSA = slave_address;                  // set slave address
  UCB0CTL1 &= ~UCSWRST;                       // Clear SW reset, resume operation
  UCB0IE = UCNACKIE;
  UCB0IE = UCRXIE;                            // Enable RX interrupt

}

after that the receive function gets called and here is function for that

TI_USCI_I2C_receive(3,array2);

void TI_USCI_I2C_receive(unsigned char byteCount, unsigned char *field){
  TI_receive_field = field;
  if ( byteCount == 1 ){
    byteCtr = 0 ;
    __disable_interrupt();
    UCB0CTL1 |= UCTXSTT;                      // I2C start condition
    while (UCB0CTL1 & UCTXSTT);               // Start condition sent?
    UCB0CTL1 |= UCTXSTP;                      // I2C stop condition
    __enable_interrupt();
  } else if ( byteCount > 1 ) {
    byteCtr = byteCount - 2 ;
    UCB0CTL1 |= UCTXSTT;                      // I2C start condition
  } else
    while (1);                                // illegal parameter
}

If anyone would be able to help me out with my problem with i2c would be greatly appreciated.above are 2 pictures to help explain my problem.After the first byte is received the data line just stays high . The left one is what i get with the MSP430F5529 and the right one is what i get with an arduino that i tried with some example code for debugging purposes. And i believe that its more like what i should be getting.does anyone know what i am doing wrong yet or have example code that i should try? If you want the header file or the c file just let me know.



  • Hello,

    I see the two code snippets but I do not see the other pictures you are referring to. In general, TI provides I2C examples inside of the TI Resource Explorer to help customers properly initialize the I2C module and get I2C communication up and running. Import one of the USCI I2C code examples I just provided and go through it to understand what would need to be modified to the code example to meet your specific needs, such as modifying the slave address.

    It may be beneficial to get the examples running with 2 Launchpads before trying to connect one to the ADS1100.

    Best regards,

    Matt

  • thank you for this reply. I did get it working now.....i'll add the code I ended up using and a picture from the logic analyzer to show the results I got. I don't know what happened to the pics I tried to add last time. My next question may be a little off topic but would u know how I would be able to get that result into a 16 bit value?

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2012, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     *
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP430F552x Demo - USCI_B0 I2C Master RX multiple bytes from MSP430 Slave
    //
    //  Description: This demo connects two MSP430's via the I2C bus. The slave
    //  transmits to the master. This is the MASTER CODE. It continuously
    //  receives an array of data and demonstrates how to implement an I2C
    //  master receiver receiving multiple bytes using the USCI_B0 TX interrupt.
    //  ACLK = n/a, MCLK = SMCLK = BRCLK = default DCO = ~1.045MHz
    //
    // ***to be used with "MSP430F55xx_uscib0_i2c_11.c" ***
    //
    //                                /|\  /|\
    //                MSP430F5529     10k  10k     MSP430F5529
    //                   slave         |    |         master
    //             -----------------   |    |   -----------------
    //           -|XIN  P3.0/UCB0SDA|<-|----+->|P3.0/UCB0SDA  XIN|-
    //            |                 |  |       |                 |
    //           -|XOUT             |  |       |             XOUT|-
    //            |     P3.1/UCB0SCL|<-+------>|P3.1/UCB0SCL     |
    //            |                 |          |                 |
    //
    //   Bhargavi Nisarga
    //   Texas Instruments Inc.
    //   April 2009
    //   Built with CCSv4 and IAR Embedded Workbench Version: 4.21
    //******************************************************************************
    
    #include <msp430.h>
    
    unsigned char *PRxData;                     // Pointer to RX data
    unsigned char RXByteCtr;
    volatile unsigned char RxBuffer[2];       // Allocate 128 byte of RAM
    
    int main(void)
    { P6DIR |= 0x01;
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
      P3SEL |= 0x03;                            // Assign I2C pins to USCI_B0
      UCB0CTL1 |= UCSWRST;                      // Enable SW reset
      UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;     // I2C Master, synchronous mode
      UCB0CTL1 = UCSSEL_2 + UCSWRST;            // Use SMCLK, keep SW reset
      UCB0BR0 = 12;                             // fSCL = SMCLK/12 = ~100kHz
      UCB0BR1 = 0;
      UCB0I2CSA = 0x48;                         // Slave Address is 048h
      UCB0CTL1 &= ~UCSWRST;                     // Clear SW reset, resume operation
      UCB0IE |= UCRXIE;                         // Enable RX interrupt
    
      while (1)
      {
        PRxData = (unsigned char *)RxBuffer;    // Start of RX buffer
        RXByteCtr = 2;                          // Load RX byte counter
        while (UCB0CTL1 & UCTXSTP);  // Ensure stop condition got sent
        UCB0CTL1 |= UCTXSTT;                    // I2C start condition
    
        __bis_SR_register(LPM0_bits + GIE);     // Enter LPM0, enable interrupts
                                                // Remain in LPM0 until all data
                                                // is RX'd
        __no_operation();                       // Set breakpoint >>here<< and
      }                                         // read out the RxBuffer buffer
    }
    
    //-------------------------------------------------------------------------------
    // The USCI_B0 data ISR is used to move received data from the I2C slave
    // to the MSP430 memory. It is structured such that it can be used to receive
    // any 2+ number of bytes by pre-loading RXByteCtr with the byte count.
    //-------------------------------------------------------------------------------
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector = USCI_B0_VECTOR
    __interrupt void USCI_B0_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCI_B0_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      switch(__even_in_range(UCB0IV,12))
      {
      case  0: break;                           // Vector  0: No interrupts
      case  2: break;                           // Vector  2: ALIFG
      case  4: break;                           // Vector  4: NACKIFG
      case  6: break;                           // Vector  6: STTIFG
      case  8: break;                           // Vector  8: STPIFG
      case 10:                                  // Vector 10: RXIFG
        RXByteCtr--;                            // Decrement RX byte counter
        if (RXByteCtr)
        {
          *PRxData++ = UCB0RXBUF;               // Move RX data to address PRxData
          if (RXByteCtr == 1)                   // Only one byte left?
            UCB0CTL1 |= UCTXSTP;                // Generate I2C stop condition
        }
        else
        {
          *PRxData = UCB0RXBUF;                 // Move final RX data to PRxData
          __bic_SR_register_on_exit(LPM0_bits); // Exit active CPU
        }
        break;
      case 12: break;                           // Vector 12: TXIFG
      default: break;
      }
    }

  • Hi,

    In order to get the results into a 16 bit value, you'd have to declare an "int" variable and copy the results into that variable.

    Best regards,

    Matt

**Attention** This is a public forum