This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP430FR5728: the availability of doubling I2C channels ?

Part Number: MSP430FR5728

Tool/software: TI C/C++ Compiler

In the Msp430fr572x family user's manual, page 530, mentions in blue :

The eUSCI_B module supports two serial communication modes:
• I2C mode
• SPI mode

If more than one eUSCI_B module is implemented on one device, those modules are named with incrementing numbers. For example, if one device has two eUSCI_B modules, they are named eUSCI0_B and eUSCI1_B.

Does this means that I have to use eUSCI_B module only as one channel for I2C and the other for SPI, or I can use both channels for I2C, or for SPI?  

Please advice.  Thanks.

-Ted 

**Attention** This is a public forum