Tool/software: Code Composer Studio
I have MSP-GANG430 programmer and it has firmware 1.62 but i want to go back to 1.55 version. can you please suggest any ideas related to this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I have MSP-GANG430 programmer and it has firmware 1.62 but i want to go back to 1.55 version. can you please suggest any ideas related to this?
Hello,
Based on Katie's comments in the thread below, you'll need to completely uninstall MSP-GANG software and install the older version.
MSP-GANG: MSP-GANG firmware (msp-gang_1_02_08_00) bug.
Regards,
James
Rohith Bachina said:Tool/software: Code Composer Studio
I have MSP-GANG programmer and it has firmware 1.62 but i want to go back to 1.55 version. can you please suggest any ideas related to this?
No, You don't have a MSP-GANG :) . What you have is MSP-GANG430, I tell this from the firmware version your description.
http://www.ti.com/tool/MSP-GANG430
I can't see FW1.55, Maybe 1.59 is also fine for you.
Hi Rohith,
Rohith Bachina said:Whenever I try to download any ot the above versions you suggested it is always 1.62. you can check it out and let me know if you have any other suggestions please
I confirmed that the latest v1.62 is always downloaded regardless of the version selected, but the MSP-GANG430 is considered obsolete. Thus, I don't have high expectations that this will get resolved. I'll still check, but it could take up to a week to learn anything.
Regards,
James
In the meantime, could you please explain why you'd like to use an earlier version of the MSP-GANG430 software? Is v1.62 working correctly? Typically, we recommend using the latest versions, so the bug fixes and device support are the most up-to-date.
Regards,
James
we are trying to use (1.62) it for our product here in our company but whenever we try to use 1.62 it is failing the process and occurring lot of other problems. when we use v1.55 it is working absolutely fine. thats why we are in need of v1.55 right now.
Hello Rohith,
Thanks for your reply. Could you provide more details about the issues you're having with v1.62? Perhaps we can get it to work. In the meantime, I'm still waiting to hear back from our software team on whether or not the older version v1.55 is available.
Regards,
James
Hello Rohith,
Unfortunately, the earlier firmware versions are not available because the MSP-GANG430 is obsolete. I'm sorry about that. Moving forward, we can try to figure out the issue you're seeing, and if that doesn't work, you may need to purchase the newer MSP-GANG for production programming.
Regards,
James
**Attention** This is a public forum