Part Number: MSP430F5529
Other Parts Discussed in Thread: LMX2595
Tool/software: Code Composer Studio
Hi Sir
1) Can anyone let me know how can I access 79x magic constants in MSP430F5529 which are 24-bit long and how to load these constants with the data which I get from TICS PRO software and I haven't found the slave select pin in MSP430F5529 to interface with LMX2595.
2) The launch pad kit is used to program the controller but once it is programmed we cannot remove the controller from the launch pad kit. In the fabrication point of view how can I load the code in the controller and interface with the slave device LMX2595.
3) In my application I am using MSP430F5529 to interface with LMX2595 to generate 17 GHz frequency. Now in order to generate different frequency in steps (17.01,17.02...) the value of fractional divider which is in the feedback path of the VCO and Phase frequency detector is to be changed. Now can I obtain this but using any switch case in programming because for each and every new frequency I need to change the entire registers values. Can I achieve this by using single micro controller.
4) Any help with respect to spi programming will be greatly appreciated.
Thanks in advance.