My customer needs to use USB and two CAN interfaces. Pin 96 (PB1) shares USB0VBUS and CAN1Tx.
Is it possible to configure pin 96 (PB1) for CAN1Tx and at the same time use USB. If yes, are the any limitations in USB usage?
Thanks
Josef
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My customer needs to use USB and two CAN interfaces. Pin 96 (PB1) shares USB0VBUS and CAN1Tx.
Is it possible to configure pin 96 (PB1) for CAN1Tx and at the same time use USB. If yes, are the any limitations in USB usage?
Thanks
Josef
Hello Josef,
Josef Alt said:Is it possible to configure pin 96 (PB1) for CAN1Tx and at the same time use USB. If yes, are the any limitations in USB usage?
Yes it's possible if USB is used as a dedicated host or device (that is no OTG). See the following screenshot from TRM.
Thanks,
Sai
**Attention** This is a public forum