Part Number: MSP430F2002
Hi champs,
after startup MCU sometimes shows a non expected behaviour (try to get more information from customer).
During this abnormal state, power consumption is significant lower (my not confirmed assumption: CPU clock is much lower than expected).
This behaviour can only be seen without JTAG debugger!
CLK is configured at beginning of code. A workaround seems to insert 2 x __no_operation() to bypass tis behaviour.
Only one __no_operation() does not work secureley!
Customer thought erratum BCL12 can be applied, but code is executed after PON, so very unlikely.
Here is code sequence:
/* Set the MCLK to 12MHz calibrated */
DCOCTL = 0; /* Select lowest DCOx and MODx settings */
BCSCTL1 = CALBC1_12MHZ; /* Set range */
DCOCTL = CALDCO_12MHZ; /* Set DCO step + modulation */
BCSCTL2 |= DIVS_2; /* SMCLK = 3 MHz */
__no_operation();
__no_operation();
Q: Why are 2 x __no_operation() needed and is this a valid workaround to ensure stable execution in mass production ?