This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6779: Using TI tools for mass production: MSP-TS430PEU128, UNIFLASH, MSP-FET, MSP-GANG

Part Number: MSP430F6779
Other Parts Discussed in Thread: MSP-TS430PEU128, UNIFLASH, MSP-FET

Hello,

My customer asked me whether the following items are good to build a mass production uC programmer or not. Could you please advise ?

Please tell me about each the item:

1. MSP-TS430PEU128: A socket board.

2. UNIFLASH: A GUI or command-line based programming application for PC.

3. MSP-FET: USB-JTAG box.

4. MSP-GANG: A stand-alone programmer.

 

The target uC is MSP430F6779IPEU.

 

The point “good to build a mass production system or not” may be not clear or not easy to agree, therefore it would be better for everyone to use different words like:

[a] The product is intended for mass-production.

[b] Neutral. It is up to users. The product is Not intended for mass-production. On the other hand, none of known fatal issues to stop it.

[c] We would advise customers not to use it for mass-production.

  

  • Hi Hideaki

    For the mass production, the best choice is the MSP-GANG.

    Several programming modes:

    • Interactive Mode – Programming while connected to PC using the MSP GANG Programmer GUI
    • Program from Image – An image can be stored, which contains configuration options and code files. This allows users to program MSP devices standalone, without a PC
    • Programming from Script – Enables developers to automate more complicated programming procedures.

    Best regards

    Gary

  • Gary,

    Thank you very much!

**Attention** This is a public forum