Part Number: MSP430F5529
Other Parts Discussed in Thread: MSP-FET
I am trying to load firmware to a custom board with MSP430F5529 via a MSP-FET Flash Emulation Tool. My circuit design was based off SLAU278AE Fig. 2-1 and the example designs at the end of the document. Board power comes from an external USB connection, which distributes 5V to the internal 3.3V LDO in the MSP430F5529. I have tested the power distribution and it works correctly.
When I attempt to load the code, first the code builds, then I get a status bar telling me that the debugger is being configured and finally I get the error "Error connecting to the target: Unknown device" with "TI MSP430 USB1/MSP430" along the window bar.
Going over the design again I found an error connecting pin 4 of the JTAG header to 5V rather than 3.3V. I ripped up the traces, wired a fix and tested. I haven't been able to discover anything else.
Schematic and Layout (GND and PWR planes not shown): https://imgur.com/a/NWxBnNw
OS: Windows 10
CCS: 9.1.0