This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FG4618: Pin compatible replacement with larger flash

Part Number: MSP430FG4618

Hi,

I've inherited a project using the MSP430FG4618. The program running on this chip leaves the chip with almost no space. (116K Flash)

Is anyone able to recommend me a replacement for this chip with these requirements:

  • Same pin count and pin functions
  • 128K Flash+
  • 8K+ RAM

Thanks.

**Attention** This is a public forum