This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2132: Absolute accuracy of internal temp sensor over temp range

Genius 12760 points

Part Number: MSP430F2132

Customer needs absolute accuracy with the internal temp sensor of MSP430F2132T.

The in the User’s Guide, section 24.2.2.1 described calibration is using two points with a tolerance of ±2°C.

Considering the MSP430 calibration values (table 24-4) can he assume that over the full temp range -40°C - +105°C the tolerance is ±2°C or can it be higher?

Regards, Bernd

**Attention** This is a public forum