This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F413: Comparator A CAO pin

Part Number: MSP430F413

Saw the above statement on the MSP430x4xx Family Users Guide (slau056b).

Does it mean that the comparator input for MSP430F413 input Pin 47 (P16/CA0) need to connect a resistor

(100K) to ground when no signal is detected.

My current design is open as shown.

  • Hello,

    The two pictures are broken. For unused pin, please follow below requirements. The unused GPIOs should be configure to port function, output direction. And left unconnected on the PC board, to reduce power consumption.

      

**Attention** This is a public forum