Other Parts Discussed in Thread: MSP430FR2153, MSP430FR2433,
Planning on using a MSP to actuate solenoid valves.
would like to send firmware updates that will generate a command to the MSP to actuate the solenoids.
I would like to send these commands using BSL or UART to the MSP.
Main concern in this sense is to make sure there’s a fall-back/fail-safe mechanism that allows to restore the device in case something goes wrong during the update (bad code, transmission interruption, …)
The way I plan to follow to ensure this is to set the reset vector to the BSL vector before starting the update so that if anything goes wrong, the watchdog would reset at that point. Would this approach be Ok?
Also would MSP430G2553 be a good choice here or could any of the FRAM devices such as MSP430FR2433 or MSP430FR2153 provide additional advantages here?
Also to finish off what is the accuracy of the built in temp sensor on the ADC of the MSP430G2553?
Your help here is much appreciated