Hi,
I'm looking for an interruptless example code to send to and receive data from EEPROM for MSP430F47186.
Also the EEPROM that we want to use supports 1Mhz I2C speed. I have checked MSP430 Module, I2C clock generator supports this speed at 8Mhz MCLK and single master mode. but on the summary they said I2C module of MSP430F47186 supports up to 400kHz. Is there any restriction other than baud rate generation to reach 1Mhz? I want to use the module at that speed.
Thanks,
BP.