Hello E2E,
I am having trouble setting an interrupt on the GPIO Port 6 pin 3 of the MSP430f5252.
My GPIO configuration is :
GPIO_PinConfig gpioPinConfigs[] = {
// ...
GPIOMSP430_P2_1 | GPIO_CFG_INPUT | GPIO_CFG_IN_INT_FALLING, /* BUTTON */
GPIOMSP430_P6_3 | GPIO_CFG_INPUT | GPIO_CFG_IN_INT_FALLING, /* IR_RX */
// ...
}
In the init, I set a callback and enable interrupts :
GPIO_setCallback(BUTTON, buttonInterruptFxn); GPIO_setCallback(IR_RX, irrxInterruptFxn); GPIO_enableInt(BUTTON); GPIO_enableInt(IR_RX);
And I have in the Project.cfg :
hwiParams.arg = 2; Hwi.create(38, "&GPIO_hwiIntFxn", hwiParams); // PORT 2 hwiParams.arg = 1; Hwi.create(36, '&GPIO_hwiIntFxn', hwiParams); // PORT 6
The interrupt for the BUTTON pin works fine but the one for the IR_RX pin doesn't work as intended.
It never goes into the irrxInterruptFxn, and it even seems to mess with other things such as a Clock.
(And if there is a way to setup interrupts without the cfg file, it would be easier to maintain)
What am I missing here ? Thanks for your help !
Clement