Other Parts Discussed in Thread: MSP430F5438A, UNIFLASH, , SEGGER
Hi,
I'm new to the MSP430 family. I just got a MSP-FET programmer/emulator for development with an existing product which uses the MSP430F5438A. When I attempt to connect to the device, the MSP-FET reports that it "Could not find the device (or the device is not supported)." I created test projects in both CCS and IAR, making sure to set the micro as the MSP430F5438A. Then, I selected the debugging tool as the MSP-FET. Both IAR and CCS report the same issue. When I attempt to program from the command line tool, MSP Flasher, it fails, while creating the attached log. The Uniflash tool also fails.
When I run MSP Flasher in DETECT mode, it locates the debugger and opens a debug session with it. Also, the green light on the MSP-FET is on and the red light blinks with activity when it is being accessed. I have both a "MSP Application UAT1" on COM7 and "MSP Debug Interface" on COM8.
The control I am attempting to program is definitely powered-up. The original software is still running on it and responds to user interaction.
I'm used to using Segger J-link-Plus with ARM processors, so this situation has me a bit befuddled. Can anyone offer any advice?
Thanks,
Jon
Log from MSPFlasher:
Tue Sep 24 15:23:06 2019: * -----/|-------------------------------------------------------------------- *
Tue Sep 24 15:23:06 2019: * / |__ *
Tue Sep 24 15:23:06 2019: * /_ / MSP Flasher v1.3.20 *
Tue Sep 24 15:23:06 2019: * | / *
Tue Sep 24 15:23:06 2019: * -----|/-------------------------------------------------------------------- *
Tue Sep 24 15:23:06 2019: *
Tue Sep 24 15:23:06 2019: * Evaluating triggers...
Tue Sep 24 15:23:06 2019: * Invalid argument for -i trigger. Default used (USB).
Tue Sep 24 15:23:06 2019: * Checking for available FET debuggers:
Tue Sep 24 15:23:06 2019: * Found USB FET @ COM8 <- Selected
Tue Sep 24 15:23:06 2019: * Initializing interface @ COM8...done
Tue Sep 24 15:23:06 2019: * Checking firmware compatibility:
Tue Sep 24 15:23:06 2019: * FET firmware is up to date.
Tue Sep 24 15:23:06 2019: * Reading FW version...done
Tue Sep 24 15:23:06 2019: * Setting VCC to 3000 mV...done
Tue Sep 24 15:23:11 2019: * Accessing device...
Tue Sep 24 15:23:16 2019: # Exit: 16
Tue Sep 24 15:23:16 2019: # ERROR: Unknown device
Tue Sep 24 15:23:16 2019: * Powering down...done
Tue Sep 24 15:23:16 2019: * Disconnecting from device...done
Tue Sep 24 15:23:16 2019: *
Tue Sep 24 15:23:16 2019: * ----------------------------------------------------------------------------
Tue Sep 24 15:23:16 2019: * Driver : closed (Internal error)
Tue Sep 24 15:23:16 2019: * ----------------------------------------------------------------------------
Tue Sep 24 15:23:16 2019: */