Tool/software: Code Composer Studio
Hello,
I have a problem with a program using driverLib on the MSP430FR5994.
I have a timer A configured in Up mode to 1 second, it works fine (I have the interruption toggle a LED), but inside I send 5 bytes by serial (9600 - 8N1).
The serial works fine, but the data arrives every two times the timer interrupts, In other words, In one interruption I don't see data on the serial, and on the next, I get the delayed data, and the new data at the same time.
Here is my code.
#include "driverlib.h"
void board_init()
{
//Set DCO Frequency to 1MHz
CS_setDCOFreq(CS_DCORSEL_0, CS_DCOFSEL_0);
//configure MCLK, SMCLK to be source by DCOCLK
CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1);
CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1);
// Set GPIO pins as out
GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0 + GPIO_PIN1);
// Set GPIO pins as input
}
void timer_init()
{
//Start timer in up mode sourced by SMCLK
Timer_A_clearTimerInterrupt(TIMER_A0_BASE);
Timer_A_initUpModeParam param = { 0 };
param.clockSource = TIMER_A_CLOCKSOURCE_SMCLK;
param.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_40;
param.timerPeriod = 25000;
param.timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_DISABLE;
param.captureCompareInterruptEnable_CCR0_CCIE = TIMER_A_CCIE_CCR0_INTERRUPT_ENABLE;
param.timerClear = TIMER_A_DO_CLEAR;
param.startTimer = false;
Timer_A_initUpMode(TIMER_A0_BASE, ¶m);
Timer_A_startCounter( TIMER_A0_BASE, TIMER_A_UP_MODE);
}
void uart_init()
{
// Configure UART pins
//Set P2.0 and P2.1 as Secondary Module Function Input.
/*
* Select Port 2d
* Set Pin 0, 1 to input Secondary Module Function, (UCA0TXD/UCA0SIMO, UCA0RXD/UCA0SOMI).
*/
GPIO_setAsPeripheralModuleFunctionInputPin( GPIO_PORT_P2,
GPIO_PIN0 + GPIO_PIN1,
GPIO_SECONDARY_MODULE_FUNCTION);
// Configure UART
EUSCI_A_UART_initParam param = { 0 };
param.selectClockSource = EUSCI_A_UART_CLOCKSOURCE_SMCLK;
param.clockPrescalar = 6;
param.firstModReg = 8;
param.secondModReg = 20;
param.parity = EUSCI_A_UART_NO_PARITY;
param.msborLsbFirst = EUSCI_A_UART_LSB_FIRST;
param.numberofStopBits = EUSCI_A_UART_ONE_STOP_BIT;
param.uartMode = EUSCI_A_UART_MODE;
param.overSampling = EUSCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION;
if (STATUS_FAIL == EUSCI_A_UART_init(EUSCI_A0_BASE, ¶m))
{
return;
}
EUSCI_A_UART_enable(EUSCI_A0_BASE);
EUSCI_A_UART_clearInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT);
// Enable USCI_A0 RX interrupt
EUSCI_A_UART_enableInterrupt(EUSCI_A0_BASE,
EUSCI_A_UART_RECEIVE_INTERRUPT); // Enable interrupt
}
int main(void)
{
//Stop watchDog Timer
WDT_A_hold(WDT_A_BASE);
board_init();
timer_init();
uart_init();
// Activate all pins changes
PMM_unlockLPM5();
__bis_SR_register(GIE);
GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
__bis_SR_register(LPM0_bits);
while (1)
{
__delay_cycles(250000); // (1/2) seg
GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN1);
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, '@');
}
}
char num[4];
int contador = 0;
#pragma vector = TIMER0_A0_VECTOR
__interrupt
void TIMER1_A0_ISR(void)
{
if (contador > 9999)
contador = 0;
num[3] = (int) (contador % 10);
num[2] = (int) ((contador / 10) % 10);
num[1] = (int) ((contador / 100) % 10);
num[0] = (int) ((contador / 1000));
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, num[0] + 48);
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, num[1] + 48);
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, num[2] + 48);
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, num[3] + 48);
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, 10);
//Toggle P1.0
GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0);
contador++;
}
uint8_t RXData = 0, TXData = 0;
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
{
switch (__even_in_range(UCA0IV, USCI_UART_UCTXCPTIFG))
{
case USCI_NONE:
break;
case USCI_UART_UCRXIFG:
RXData = EUSCI_A_UART_receiveData(EUSCI_A0_BASE);
GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN1);
switch (RXData)
{
case 'a':
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, 'h');
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, 'i');
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, '0');
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, '1');
break;
default:
EUSCI_A_UART_transmitData(EUSCI_A0_BASE, RXData);
break;
}
break;
case USCI_UART_UCTXIFG:
break;
case USCI_UART_UCSTTIFG:
break;
case USCI_UART_UCTXCPTIFG:
break;
}
}
Thank you.