Hi,
What will happen to RAM of MSP432E401Y on software reset using SysCtlReset() API?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What will happen to RAM of MSP432E401Y on software reset using SysCtlReset() API?
Thanks
Hi seong,
Did you means to say that previously allocated dynamic memory is not reset?
If yes then how to reset RAM memory when device reset? is there any other method for erase RAM when Microcontroller reset?
Thanks,
Dinkar
Hi,
ok, i reset memory using memset().
char * test = malloc(100); // suppose test allocated memory block on 0x20007894.
then if i reset code using SysCtlReset() API then can my code able to allocate new dynamic block on that location (0x20007894)?
Thnaks
dinkar
Hi Dinkar,
If you were to reset your program by calling SysCtlReset(), then you will the same memory block allocated to *test. This is since TIRTOS will reinitialize itself and reset its entire state, including the state of allocated heap memory, once you run BIOS_start() from main(). This is regardless of whether the RAM state is retained or not, since all of your code is placed in flash during linking by default.
Given the compiler should only use RAM for temporary storage of data, it shouldn't matter to your code once it resets whether the RAM was in a non-reset state. The RAM is used for automatic allocation of data for the stack which is routinely reused by the program as data goes in and out of scope. It is also used for dynamic allocation of data which as explained above doesn't require the state of RAM to be fully clean, since the RTOS will reinitialize its heap memory table.
You can test this behavior for yourself by running the following test code in the mainThread() of your program:
//memory/reset testing
volatile int i =0;
while(i==0);
int* y;
y = (volatile int*)(0x20000000+0x00040000-250);
*y = 0x3010;
someHeap = (int*)malloc(400);
while(i==0){
}
SysCtlReset();
You will need to adjust the memory map of your program in your .cmd file like so to be totally safe:
MEMORY
{
FLASH (RX) : origin = 0x00000000, length = 0x00100000
SRAM (RWX) : origin = 0x20000000, length = 0x00040000-250
SRAM_EX (RWX) : origin = 0x20000000+0x00040000-250, length = 250
}
If you run that code you will get stuck at the first while(i==0). However, in debug mode you can point the PC to any executable instruction, and you can use that functionality to jump over the while(i==0) loops. If you jump to the second section, you'll see that the RAM is written and the malloc called to give a pointer to someHeap. Once you have recorded the heap memory address for reference, you can jump to the SysCtlReset() call. That should bring you back to the first while loop. At this point, you can check to see the data previously written to the address y to verify that the RAM was not reset. Then, if you jump back to the malloc, you'll observe that despite the RAM being fully retained, the RTOS will give someHeap the same memory block as the first iteration pre-reset.
Let me know if you need more clarification on the explanation above, or if you have further questions on SysCtlReset().
Regards,
Michael
**Attention** This is a public forum