Part Number: MSP430FR5949
Other Parts Discussed in Thread: PMP40441, , TUSB422, BQ25713, BQ34Z950
Tool/software: Code Composer Studio
hi,
we need support in PMP40441 software (we purchased it from TI direct through our US client),
- the PMP40441 software.zip
- PMP40441 software.zip is extracted
- it has 4 project file within the the folder in different place (see the image 1)

- we are working in MSP430fr5949, why you have supplied four project files?
- even these project files are having more errors while compiling,
- in the four project file which is the right file we can use for our application(we are usingmsp430fr5949)
- there are two main file, so which main file i have to use
- one main file is under PMP40441
- another main file is under TUSB422_MSP432P401R
- so please guide me to open the right project file for our msp430fr5949 based project; else give me a new correct error free file to operate.