Part Number: MSP430I2041
Other Parts Discussed in Thread: MSP-FET
Hello Ti community and Ti experts, i am trying to receive the HEX sequence of 50 bytes that gives the measures. We did a layout with the Integrated Circuit MSPI2041 and we are trying to communicate the TX and RX with and 3v3 micro using arduino IDE.
For the serial communication, we are using 9600 bauds/s that is the speed of the MSP. We send a password of 26 bytes when the board with the msp starts, that is:{0xFE,0xFE,0xFE,0xFE,0x68,0x99,0x99,0x99,0x99,0x99,0x99,0x68,0x23,0x0A,0x60,0x00,0x34,0x12,0x78,0x56,0xBC,0x9A,0xF0,0xDE,0x2B,0x16}. The board powers the micro, so when the board starts the micro starts sending the request.
And after that, a loop starts sending a request of 18 bytes that is {0xFE,0xFE,0xFE,0xFE,0x68,0x99,0x99,0x99,0x99,0x99,0x99,0x68,0x23,0x02,0x61,0x00,0xEC,0x16} . And we wanted to receive after that a sequence of 50 bytes that indicate the measures but we are receving 0 in all values.
Don't know what to do anymore, already tried to send the password first, after that the request and all that is received are zero values.