Hi Team,
What is the Max VIH threshold of SBWTCK (pin 4) of MSP430FR2155TPR when VCC is 3.3V?
What I only could find from datasheet is section 5.13.5, table 5-11
VCC 2.0V -> VIH Threshould Max is 1.5V (= 0.7 times of 2.0V)
VCC 3.0V -> VIH Threshould Max is 2.25V (= 0.7 times of 3.0V)
So if I use 0.75 times of VCC,
Does it mean VCC 3.3V -> VIH Threshould Max is 2.475V (= 0.7 times of 3.3V) ?
Best regards,
Andy Chu