Part Number: MSP430FR2476
Hi,
I've got a problem with MSP430FR2476 when I use memory allocation. I'm using IAR 7.12.4
Basically, the "malloc()" function doesn't allocate the memory. I did a test program and noted the values of the first and second positions of the vector doesn't receive the correct inicialization, like this picture:
I've tried to set the Heap size on the compiler settings, like this:
I've tried to set the Heap size on the linker file, but the result are the same. If I change the type of "p" or set 0 on the Heap size, the vector doesn't receive any value.