This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hello
I have a following problem : when i try to use pin oscillator with conjunction with pwm then nothing happen on pwm output
Timer_A_PWMConfig pwm1 = {0};
pwm1.clockSource = TIMER_A_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK; // when i put here SMCLK or ACLK all work fine
pwm1.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_64;
pwm1.compareRegister=TIMER_A_CAPTURECOMPARE_REGISTER_1;
pwm1.compareOutputMode=TIMER_A_OUTPUTMODE_TOGGLE;
P3REN |= 1<<7; // pu&pd
P3SELC |= 1<<7; // additional port function
CAPTIO0->CTL |= 3<<4 | 7<<1 | 1<<8; //captio function
GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2, GPIO_PIN4, GPIO_PRIMARY_MODULE_FUNCTION); // p2.4 as pwm
printf("timer period (write below) ? \n");
while(1)
{
if (scanf("%d",&max)) { // if something entered then do
pwm1.timerPeriod=max;
pwm1.dutyCycle=pwm1.timerPeriod/2;
Timer_A_generatePWM(TIMER_A0_BASE, &pwm1);
printf("timer period equals now %d and duty %d \n",max,pwm1.dutyCycle);
printf("timer period (write below) ? \n");
}
}
Please understand that this code is incomplete just essence.
I have noticed that during debugging clock source of TIMERA0 is different from what i have programmed. Simply don't understand. So how can i run this code?
Hi,
Please take a look at this similar E2E thread, and compare the code that you have with the code that the E2E poster has provided:
Let me know if that doesn't work for you.
Regards,
Michael
Hi,
I assume that you have resolved your issue since I have not heard back from you. If not, feel free to post a response to this thread, or open a new thread regarding this issue.
Regards,
Michael
**Attention** This is a public forum