I have configured my MSP432 to use the ADC14 module. I have an input signal of ~1.5 V going into Pin 5.5. The MSP432 got very hot and eventually the probe could no longer connect. I checked for any shorts but did not find any; I have only two wires connecting to the GPIO - GND and an amplified output of a temperature sensor. I am no longer able to upload my builds to run on the device; I get an error that an invalid response was received by the XDS110 debug probe (-261 @ 0x0). I believe it is the same issue that was happening here. Any help would be much appreciated.
Thanks!