Hi,
I just received my ez430 chronos, and while reviewing the documentation I realized I just can't find information on how the acceleration sensor axis are positioned. The default firmware shows this behaviour (could please someone confirm this is the expected behaviour?):
1- With the watch screen in horizontal position looking upwards, the X and Y readings are approximately zero.
2- If you tilt the watch sideways the Y reading varies, going up to 0.85 and then back to zero when the screen is again horizontal but looking downwards.
3- If you tilt the watch backwards (i.e. rotate screen towards you) the X reading varies, going up to 0.88 and then back to zero when the screen is again horizontal but looking downwards.
(so far this makes sense to me)
4- In the position described in (1) the Z reading is approx. 0.40, if you start to turn the watch towards you the reading goes down to zero, which is reached when the screen is facing you (about 45º turn from the initial position). If you continue turning the watch until the screen is facing downwards, the reading is 1.40.
Any help understanding why the Z reading behaves so differently from the other axis will be very welcome.
Thanks.