Need some help with Timer B for PWM on MSP-EXP430F5529 LaunchPad. I've setup PWM with Timer A, with output to P1.2 with no issues. When I try to set the same thing up for Timer B P3.5 I don't get any PWM signal. Below are the codes for both the Timer A and Timer B. the data sheet for the MSP430F5529 shows the CCR5 for the time block. I'm sure I'm missing something but not sure what. Any help/suggestions would be appreciated.
int main(void) {
WDTCTL = WDTPW + WDTHOLD; //Disable the Watchdog timer for our convenience.
P1DIR |= BIT2; //Set pin 1.2 to the output direction.
P1SEL |= BIT2; //Select pin 1.2 as our PWM output.
TA0CCR0 = 7000; //Set the period in the Timer A0 Capture/Compare 0 register to 7000 us.
TA0CCTL1 = OUTMOD_7; //TACCR1 reset/set mode
TA0CCR1 = 350; //The period in microseconds that the power is ON. It translates to a 5% duty cycle.
TA0CTL = TASSEL_2 + MC_1; //TASSEL_2 selects SMCLK as the clock source, and MC_1 tells it to count up to the value in TA0CCR0.
// __bis_SR_register(LPM0_bits); //Switch to low power mode 0.
int main(void) {
WDTCTL = WDTPW + WDTHOLD; //Disable the Watchdog timer for our convenience.
P3DIR |= BIT5; //Set pin 3.5 to the output direction.
P3SEL |= BIT5; //Select pin 3.5 as our PWM output.
TB0CCR0 = 7000; //Set the period in the Timer B0 Capture/Compare 0 register to 7000 us.
TB0CCTL1 = OUTMOD_7; //TBCCR1 reset/set mode
TB0CCR5 = 350; //The period in microseconds that the power is ON. It translates to a 5% duty cycle.
TB0CTL = TBSSEL_2 + MC_1; //TBSSEL_2 selects SMCLK as the clock source, and MC_1 tells it to count up to the value in TB0CCR0.
// __bis_SR_register(LPM0_bits); //Switch to low power mode 0.