Part Number: MSP-EXP430FG4618
Other Parts Discussed in Thread: MSP430F2013, UNIFLASH, MSP430F1612, MSPBSL, MSP430F4618, MSP430FG4618, MSP430FG4619, MSP430-FLASHER
Tool/software: WEBENCH® Design Tools
Hi,
Whilst in the process of trying to isolate issues with the MSP430-ELF-GCC (8.3.0.16) based toolchain, running on Ubuntu 19.10, I decided to attempt compilation using the TI Cloud Tools.
My objective is to compare the output binaries produced from the TI and GCC compilers, so that I can run MSP430-ELF-DUMP and MSP-ELF-OBJCOPY on the binaries to help me get to the bottom of the apparent MSP430F2013 (on a MSP-EXP430FG4618 experimenter board) flash corruption, which I have come up against, whilst attempting to program it using an MSP-FET430UIF tool.
When I attempted to copy the blink.out file from the TI Cloud Tools CCS IDE, on about three occasions now, it simply crashes and completely freezes the OS.
The only way I can recover, is to reboot my laptop.
Further, for some unknown reason, every now and then, when I click on the CCS Cloud button, it comes back with the message:
104 - Login Failed: Maximum login attempts reached, please retry later.
The only way I can recover from this, is to switch from Firefox to Chromium browser, or reboot my machine.
I would suggest that this is a critically serious issue, which needs to be looked into and would like to ask how I can save/export/download the binary files, generated by the TI Cloud Tools, to my laptop please.
Thanking you in advance.
Best Regards,
Jonathan Roberts