Part Number: MSP430FR6989
Hello
I am trying to read from 4 ADC channels every 10 secs to gas sensors, temperature etc. The following is the code I am using.
void Init_ADC (void)
{
REFCTL0 &= 0x00;
ADC12CTL0 = ADC12ON | ADC12MSC | ADC12SHT0_8;
ADC12CTL1 |= ADC12SHP + ADC12CONSEQ_1;
ADC12CTL2 |= ADC12RES_2 + ADC12PWRMD;
ADC12MCTL0 = ADC12VRSEL_4 + ADC12INCH_1; // A1 VeRef
ADC12MCTL1 = ADC12VRSEL_4 + ADC12INCH_7; // A7 ADC
ADC12MCTL2 = ADC12VRSEL_4 + ADC12INCH_6; // A6 ADC
ADC12MCTL3 = ADC12VRSEL_4 + ADC12INCH_5; // A5 ADC
ADC12MCTL4 = ADC12VRSEL_4 + ADC12INCH_4 + ADC12EOS; // A4 ADC
ADC12CTL0 &= ~ADC12ENC;
_delay_cycles(1000);
}
void Enable_ADC (void)
{
while(ADC12CTL1 & ADC12BUSY);
ADC12IER0 |= ADC12IE4;
ADC12CTL0 |= ADC12ENC | ADC12SC;
}
void Disable_ADC (void)
{
ADC12IER0 &= ~ADC12IE4;
ADC12CTL0 &= ~(ADC12ENC | ADC12SC);
}
Should I disable the ADC and enable them every 10 seconds using a Timer or should just let the ADC run forever? I want to know which is a better approach.
1. ADC runs continuously and sends results like below in the ISR and then read in the timer every 10 seconds.
#pragma vector = ADC12_VECTOR
__interrupt void ADC12_ISR(void)
{
result1 = +=ADC12MEM1;
result2 = +=ADC12MEM2;
result3 = +=ADC12MEM3;
result4 = +=ADC12MEM4;
ADC_Flag = TRUE;
}
__interrupt void Timer0_A0_ISR (void)
{
TA0CCR0 += 40960; // Add 10 Second Offset to TA0CCR0
if(ADC_Flag == TRUE)
myprintf("ADC1: %d, ADC2: %d, ADC3: %d, ADC3: %d\n", result1, result2, result3, result4); // print to uart
}
2. The ADC is enabled every 10 secs through Timer and disabled after reading.
#pragma vector = ADC12_VECTOR
__interrupt void ADC12_ISR(void)
{
result1 = +=ADC12MEM0;
result2 = +=ADC12MEM0;
result3 = +=ADC12MEM0;
result4 = +=ADC12MEM0;
Disable_ADC();
ADC_Flag == TRUE
__bic_SR_register_on_exit(LPM0_bits | GIE);
}
__interrupt void Timer0_A0_ISR (void)
{
TA0CCR0 += 40960; // Add 10 Second Offset to TA0CCR0
Enable_ADC();
}
int main (void)
{
__bis_SR_register(LPM0_bits | GIE);
if(ADC_Flag == TRUE)
myprintf("ADC1: %d, ADC2: %d, ADC3: %d, ADC3: %d\n", result1, result2, result3, result4); // print to uart
}
I am not an engineer or an experienced programmer. So please try to explain in detail. Also please let me know if the ADC configuration is correct.