Part Number: MSP432E401Y
Hello,
I am attempting to run the SimpleLink spimaster and spislave example code running on two MSP432E401Y LaunchPad platforms from the latest SimpleLink SDK (version 3.30.0.22). I can only get the example code to run correctly if I reverse the MOSI and MISO pins between the master and slave devices - the text messages exchanged between the master and slave are displayed correctly. If I connect MOSI->MOSI and MISO->MISO the example appears to run but the text messages transmitted between the master and slave are blank. My understanding of SPI convention is the master MOSI should be connected to the slave MOSI pin and vice versa (slave MISO to master MISO). I am using the examples "out of the box": with no changes. Please provide guidance on this issue. Is there a bug in the example code or am I missing something?
Regards,
Tim