Hi,
I'd like to create a custom USB BSL for the MSP430F6638. I downloaded source for some BSLs at http://www.ti.com/tool/MSPBSL#step3. I noticed that the zip file does not include source for USB BSLs. Is there any source code out there to start with customizing the USB bootloader?
If there is not available source for any USB bootloaders, I will likely customize a UART bootloader instead. I currently use CCS as my IDE. In this post, Katie suggested starting with the F5438A BSL source code. I'm guessing this is synonymous with the source for F543xA (CCS_BSL_Source/CCS_v5_MSP430F543xA_TA_UART), as available in the latest zip file. Is this a good starting point to develop a custom bootloader for the F6638? Or should I start somewhere else?
Thank you!
Jesse Bahr