Part Number: EVM430-FR6043
Other Parts Discussed in Thread: UA741
Hi Team, I would like seek help with my customers application. Below is his inquiry, I hope you could help us. Thank you in advance.
Customers Inquiry:
"I am using the EVMFR6043 with a single 200 kHz transducer to take water depth measurements between 0 and 5 meters. I have loaded the water demo application onto the EVM and am trying to take measurements with USS Design Center. However I see that it will not let me use frequencies below 772 kHz. From what I understand the EVM is meant for flow metering applications in small pipes and does not have the power to drive the transducer at longer distances. I would like to create an external amplifier to interface the transducer and the EVM. Would this be possible? Also, does the EVM support a 200 kHz transducer"