Part Number: MSP430F477
Can you clarify what the maximum external Vref voltage is for the device? The spec shows max Vref=AVcc+0.2V in the DAC section and another value listed in the ADC section states max Vref=1.5V.
Regards Bernd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F477
Can you clarify what the maximum external Vref voltage is for the device? The spec shows max Vref=AVcc+0.2V in the DAC section and another value listed in the ADC section states max Vref=1.5V.
Regards Bernd
Hello Bernd,
As you've observed, the maximum external reference voltage depends on the specific module you're wanting to use. Let's assume you're using the DAC but not the ADC, and the Vref voltage is AVCC + 0.2V. This will be fine since you're not enabling the ADC module. I hope this makes sense.
Regards,
James
Hi James,
From your response I believe the Vref on the DAC and Vref on the ADC are separate circuits. The DAC Vref is derived from the AVcc input and not the Vref (Pin 60). Is this correct?
The recommended external Vref for the ADC is half scale of the AVcc input voltage to the uC. If AVcc is 2.8V then the max input to Vref (Pin 60) is 1.4V. Is this correct?
I've found a circuit in our library that has the external Vref at 3.0V (Pin 60) on the MSP430F477. I want to make sure the device is not overstressed. This design uses both the DAC and ADC circuits.
Daniel (supporting Jamie)
Hi Jamie,
Daniel Studer said:From your response I believe the Vref on the DAC and Vref on the ADC are separate circuits. The DAC Vref is derived from the AVcc input and not the Vref (Pin 60). Is this correct?
It depens on how you configure the reference for the DAC. As you can see from the user's guide, the DAC can use either AVCC as the reference, the 1.2 V reference from the SD16 ADC module or an external reference. Keep in mind that this is different than the 1.5 V or 2.5 V voltage reference in the ADC12 module.
Daniel Studer said:The recommended external Vref for the ADC is half scale of the AVcc input voltage to the uC. If AVcc is 2.8V then the max input to Vref (Pin 60) is 1.4V. Is this correct?
Which ADC are you referring to? ADC12 or SD16? This information should be provided in the datasheet and/or user's guide.
Regards,
James
**Attention** This is a public forum