Part Number: MSP430F6779A
I'm considering to use LPM3 and LPM3.5 on MSP430F6779A while power supply and battery we have selected are supply voltage in 3.3 V. Therefor I would like to find actual supply currents in operating temp @50℃. But in data sheet (Refer to data sheep no. SLAS982A <page 29>) did not specify value in such conditions I mentioned to.
So my question is what are the numbers of Supply currents for these two low power modes; LPM3 (Crystal mode) and LPM3.5 in following conditions?
- Maximum supply current @25℃, Vcc = 3.3 V
- Typical and Maximum supply current @50℃, Vcc = 3.3 V
And how can I calculate or estimate numbers of those supply currents?