Part Number: MSP430F67641
Hi,
I am looking for a document that shows the maximum recommended re-flow profile temperature for MSP430F67641.
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F67641
Hi,
I am looking for a document that shows the maximum recommended re-flow profile temperature for MSP430F67641.
Best Regards
I am also curious if it's OK to solder a programmed MSP with a reflow oven at over 245°C.
If it can damage the memory program, then what is the maximum temperature for the programmed MSP.
Hello Moshen,
You should find your answers in the AN-2029 Handling and processing recommendations guide
This document is the general recommendation for Reflow Soldering. I could not find any information about a programmed component.
Anybody has an experience about reflow soldering of a programmed MSP?
Hi Mohsen,
I was able to finally trackdown the information you are looking for.
The specification is in section 2.2 of the MSP430 FRAM Quality and Reliability application report.
You will need to follow the JEDEC J-STD-020 standard with peak reflow temperatures not higher than classified on the device label on the shipping boxes or reels.
**Attention** This is a public forum