This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR2433: Trouble using UART P2.5 and P2.6 for UART Standard Transceiver Example

Part Number: MSP-EXP430FR2433
Other Parts Discussed in Thread: MSP430FR2433

Hi,

I am trying to configure the standard transceiver example on TI Resource Explorer to work on the P2.5/P2.6 instead of P1.4/P1.5. I got it to work with Port 1 Configurations but am having trouble using P2. Here is the code i'm using. 

#include "driverlib.h"
#include <msp430fr2433.h>


//******************************************************************************
// UART Initialization *********************************************************
//******************************************************************************

#define LED_OUT P1OUT
#define LED_DIR P1DIR
#define LED_PIN BIT0

#define SMCLK_115200 0
#define SMCLK_9600 1

#define UART_MODE SMCLK_9600//

void initUART()
{
// Configure USCI_A0 for UART mode
UCA1CTLW0 |= UCSWRST; // Put eUSCI in reset
#if UART_MODE == SMCLK_115200

UCA1CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate Setting
// Use Table 21-5
UCA1BRW = 8;
UCA1MCTLW |= UCOS16 | UCBRF_10 | 0xF700; //0xF700 is UCBRSx = 0xF7

#elif UART_MODE == SMCLK_9600

UCA1CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate Setting
// Use Table 21-5
UCA1BRW = 104;
UCA1MCTLW |= UCOS16 | UCBRF_2 | 0xD600; //0xD600 is UCBRSx = 0xD6
#else
# error "Please specify baud rate to 115200 or 9600"
#endif

UCA1CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA1IE |= UCRXIE; // Enable USCI_A1 RX interrupt
}

//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************

void initGPIO()
{
LED_DIR |= LED_PIN;
LED_OUT &= ~LED_PIN;

// Configure GPIO
P2SEL1 &= ~(BIT6 | BIT5); // USCI_A1 UART operation
P2SEL0 |= BIT6 | BIT5;

// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
}

void initClockTo16MHz()
{
// Configure one FRAM waitstate as required by the device datasheet for MCLK
// operation beyond 8MHz _before_ configuring the clock system.
FRCTL0 = FRCTLPW | NWAITS_1;

__bis_SR_register(SCG0); // disable FLL
CSCTL3 |= SELREF__REFOCLK; // Set REFO as FLL reference source
CSCTL0 = 0; // clear DCO and MOD registers
CSCTL1 &= ~(DCORSEL_7); // Clear DCO frequency select bits first
CSCTL1 |= DCORSEL_5; // Set DCO = 16MHz
CSCTL2 = FLLD_0 + 487; // set to fDCOCLKDIV = (FLLN + 1)*(fFLLREFCLK/n)
// = (487 + 1)*(32.768 kHz/1)
// = 16 MHz
__delay_cycles(3);
__bic_SR_register(SCG0); // enable FLL
while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // FLL locked

CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;
}

//******************************************************************************
// Main ************************************************************************
// Enters LPM0 if SMCLK is used and waits for UART interrupts. If ACLK is used *
// then the device will enter LPM3 mode instead. The UART RX interrupt handles *
// the received character and echoes it. *
//******************************************************************************

int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop Watchdog

initGPIO();
initClockTo16MHz();
initUART();

#if UART_MODE == SMCLK_9600
__bis_SR_register(LPM3_bits + GIE); // Since ACLK is source, enter LPM3, interrupts enabled
#else
__bis_SR_register(LPM0_bits + GIE); // Since SMCLK is source, enter LPM0, interrupts enabled
#endif
__no_operation(); // For debugger
}

//******************************************************************************
// UART Interrupt ***********************************************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A1_VECTOR
__interrupt void USCI_A1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A1_VECTOR))) USCI_A1_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA1IV, USCI_UART_UCTXCPTIFG))
{
case USCI_NONE: break;
case USCI_UART_UCRXIFG:
while(!(UCA1IFG&UCTXIFG));
UCA1TXBUF = UCA1RXBUF;
__no_operation();
break;
case USCI_UART_UCTXIFG: break;
case USCI_UART_UCSTTIFG: break;
case USCI_UART_UCTXCPTIFG: break;
}
}

  • Hi Kirushigan,

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2014, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     *
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //   MSP430FR243x Demo - eUSCI_A1 UART echo at 9600 baud using BRCLK = 16MHz
    //
    //  Description: This demo echoes back characters received via a PC serial port.
    //  SMCLK/ DCO is used as a clock source and the device is put in LPM3
    //  The auto-clock enable feature is used by the eUSCI and SMCLK is turned off
    //  when the UART is idle and turned on when a receive edge is detected.
    //  Note that level shifter hardware is needed to shift between RS232 and MSP
    //  voltage levels.
    //
    //  The example code shows proper initialization of registers
    //  and interrupts to receive and transmit data.
    //  To test code in LPM3, disconnect the debugger.
    //
    //  ACLK = REFO = 32768Hz, MCLK = DCODIV = SMCLK = 16MHz.
    //
    //                MSP430FR2433
    //             -----------------
    //         /|\|                 |
    //          | |                 |
    //          --|RST              |
    //            |                 |
    //            |                 |
    //            |     P2.6/UCA1TXD|----> PC (echo)
    //            |     P2.5/UCA1RXD|<---- PC
    //            |                 |
    //
    //   Ling Zhu
    //   Texas Instruments Inc.
    //   Nov 2019
    //   Built with IAR Embedded Workbench v7.10 & Code Composer Studio v7.3
    //******************************************************************************
    
    #include <msp430.h>
    
    void Init_GPIO();
    
    int main(void)
    {
      WDTCTL = WDTPW | WDTHOLD;                // Stop watchdog timer
    
      // Configure GPIO
      Init_GPIO();
      PM5CTL0 &= ~LOCKLPM5;                    // Disable the GPIO power-on default high-impedance mode
                                               // to activate 1previously configured port settings
    
      // Configure one FRAM waitstate as required by the device datasheet for MCLK
      // operation beyond 8MHz _before_ configuring the clock system.
      FRCTL0 = FRCTLPW | NWAITS_1;
    
      __bis_SR_register(SCG0);                           // disable FLL
      CSCTL3 |= SELREF__REFOCLK;                         // Set REFO as FLL reference source
      CSCTL0 = 0;                                        // clear DCO and MOD registers
      CSCTL1 &= ~(DCORSEL_7);                            // Clear DCO frequency select bits first
      CSCTL1 |= DCORSEL_5;                               // Set DCO = 16MHz
      CSCTL2 = FLLD_0 + 487;                             // DCOCLKDIV = 16MHz
      __delay_cycles(3);
      __bic_SR_register(SCG0);                           // enable FLL
      while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));         // FLL locked
    
      CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;         // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                                         // default DCOCLKDIV as MCLK and SMCLK source
    
      // Configure UART pins
      P2SEL0 |= BIT5 | BIT6;                             // set 2-UART pin as second function
    
      // Configure UART
      UCA1CTLW0 |= UCSWRST;
      UCA1CTLW0 |= UCSSEL__SMCLK;
    
      // Baud Rate calculation
      // 16000000/(16*9600) = 104.167
      // Fractional portion = 0.167
      // User's Guide Table 14-4: UCBRSx = 0x11
      // UCBRFx = int ( (104.167-104)*16) = 2
      UCA1BR0 = 104;                             // 16000000/16/9600
      UCA1BR1 = 0x00;
      UCA1MCTLW = 0x1100 | UCOS16 | UCBRF_2;
    
      UCA1CTLW0 &= ~UCSWRST;                    // Initialize eUSCI
      UCA1IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
    
      __bis_SR_register(LPM3_bits|GIE);         // Enter LPM3, interrupts enabled
      __no_operation();                         // For debugger
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=USCI_A1_VECTOR
    __interrupt void USCI_A1_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(USCI_A1_VECTOR))) USCI_A1_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      switch(__even_in_range(UCA1IV,USCI_UART_UCTXCPTIFG))
      {
        case USCI_NONE: break;
        case USCI_UART_UCRXIFG:
          while(!(UCA1IFG&UCTXIFG));
          UCA1TXBUF = UCA1RXBUF;
          __no_operation();
          break;
        case USCI_UART_UCTXIFG: break;
        case USCI_UART_UCSTTIFG: break;
        case USCI_UART_UCTXCPTIFG: break;
        default: break;
      }
    }
    
    void Init_GPIO()
    {
        P1DIR = 0xFF; P2DIR = 0xFF; P3DIR = 0xFF;
        P1REN = 0xFF; P2REN = 0xFF; P3REN = 0xFF;
        P1OUT = 0x00; P2OUT = 0x00; P3OUT = 0x00;
    }
    
    

    Ling

**Attention** This is a public forum