Dear Team,
We are thinking to use MSP430FR2476 in our new appliation where we need to use
a) 4 SPI's 2 to work simaltaneouly, out of four 2 are in slave mode and two are in master mode,
i.e.
i) 1 spi of msp430 (as slave) with one communication card say card 1 (as master)
ii) 1 spi of msp430 (as slave) with other communicatino card say card 2(as master)
iii) 2 spi of msp430 (as master) with 2 different ADC's say adc1 and adc2
b) 2 I2C at (400 kbps)
c) 2 UART
Also please let us know where spi baud rate calculation is mentioned in datasheet as i could not able to find that
Thanks,
Ashish