Part Number: TSS721A
Dear Sir,
I will test the TSS721A but I don't have any MBUS- master signal generator.
Do you have any idea to generate it or supply any manufracturer of MBUS master module?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSS721A
Dear Sir,
I will test the TSS721A but I don't have any MBUS- master signal generator.
Do you have any idea to generate it or supply any manufracturer of MBUS master module?
Hi Gordon,
MBUS protocol maybe need implement yourself.
This post maybe useful for you:
https://e2e.ti.com/support/archive/internal/int-msp430/f/167/t/327065?tisearch=e2e-sitesearch&keymatch=MBUS%20430
Best Regards
Johnson
Hi Johnson,
I can't entry the wesite.
It show "Access Denied (Note: a common reason this message is displayed is because the thread was deleted)".
Could you copy the screen to me?
Hi Gordon,
The information in this post is to answer that we don't have MBUS and need users to implement themselves.
Useful information in this post :
----------------------------------------------------
I talked to our metering team and unfortunately it does not sound like we have any software examples for using the TSS721. They said this is basically just a translator of the MBUS signals into something that can be handled by the UART module, but other than this, unfortunately the MBUS protocol processing I think you are going to have to implement yourself.
-----------------------------------------------------
Best Regards
Johnson
**Attention** This is a public forum