Part Number: MSP430F413
Tool/software: Code Composer Studio
I need code compiler, DS2762 library file for MSP430F413
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F413
Tool/software: Code Composer Studio
I need code compiler, DS2762 library file for MSP430F413
Hello,
I'm assuming that you're referring to Maxim's DS2762 High-Precision Li+ Battery Monitor with Alerts device. It seems to communicate using the 1-wire interface, so I would suggest taking a look at the following resources:
Single-Wire Communication Host With MSP430™ MCUs
Memory Emulation Using 1-Wire® Communication Protocol
We don't seem to offer a library for 1-wire communication, so you would need to develop the firmware.
I would also take a look at our Battery Management solutions. Our devices may use a different communication protocol and there may be a reference design that uses MSP430 which should make your development easier.
Regards,
James
g g1 said:can i get any sample code for 1 wire
Did you look at the two resources linked above? The first one should have example code.
Regards,
James
**Attention** This is a public forum