Tool/software: Code Composer Studio
Hi!
I have some questions regarding Hilbert mode and ATOF calculation:
1. When the Hilbert absTOF computation mode is used, is it applied after the interpolation of the ADC signal?
2. How should I select the correct order(length) off the Hilbert coefficients? See image below for two different orders.
3. Are the UPS/DNS values calculated using the continuous slope by the Hilbert transform, or is it finding peaks from the raw signal like in the Lobe-mode? See the image below, will it select a value from the red or blue circle(or other)?
The image above shows the raw ADC signal(blue) with two different Hilbert transforms applied. Orange: filter order 12, green: filter order 30.
Thanks in advance