If have this error that I've found in three other threads:
CORTEX_M4_0: * WARNING *: The connected device is not MSP432P401R
CORTEX_M4_0: GEL Output: Memory Map Initialization Complete
CORTEX_M4_0: GEL Output: Halting Watchdog Timer
CORTEX_M4_0: Error initializing flash programming: Your XMS432P401R material is no longer supported. We recommend you moving to production-quality MSP432P401R/M silicon by ordering samples at www.ti.com/product/MSP432P401R.
CORTEX_M4_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
Which looks like my MSP432 is dead. Mainly the advice seems to be to factory reset, which I did and received the prompt to exit debug and power cycle. After doing so the above error still comes up. This happened after trying to make my dcoFrequency go to 48MHz. I haven't found a solution in any threads,