This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: How can i erase the flash?

Part Number: MSP432E401Y

Hello,

For updating a firmware image how exactly would this work in the field, if iam using ethernet as the updaters transport layer.I have a launchpad for a MSP432E401Y and iam following the first link below but when i get to Task4. Instruction 1 using ethernet it assumes that the MCU's flash is erased.The only way the BSL scripter can erase memory is through the USB DFU Comm. per Table.1 page 5 in the second link what exactly are my options here to be able to update the firmware 100% using ethernet?

Thanks any input is appreciated

http://dev.ti.com/tirex/content/simplelink_academy_msp432e4sdk_1_15_00_00/modules/msp432e4_bootloader/msp432e4_bootloader.html

https://www.ti.com/lit/ug/slau655f/slau655f.pdf

**Attention** This is a public forum