This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430G2553: msp430

Part Number: MSP430G2553


Tool/software: Code Composer Studio

how to resend  the received  data from the serial port to  UART in MSP430G2553

  • Sir,

    Thank you for your reply 

    This is my code to  receive the  transmitted data from terminal  to MSP430G2553 without interrupt  and  using URXIFG0 flag.But not setting the mentioned flag and not getting the expected output. I am trying to do without using interrupt.

    #include "msp430g2553.h"

    #define TXLED BIT0
    #define RXLED BIT6
    #define TXD BIT2
    #define RXD BIT1

    unsigned int URXIFG0;
    unsigned int i;


    int main(void)
    {
    WDTCTL = WDTPW + WDTHOLD; // Stop WDT
    DCOCTL = 0; // Select lowest DCOx and MODx settings
    BCSCTL1 = CALBC1_1MHZ; // Set DCO
    DCOCTL = CALDCO_1MHZ;
    P1DIR = BIT0;
    P1OUT = BIT0+BIT6;

    P2DIR |= 0xFF; // All P2.x outputs
    P2OUT &= 0x00; // All P2.x reset
    P1SEL |= RXD + TXD ; // P1.1 = RXD, P1.2=TXD
    P1SEL2 |= RXD + TXD ; // P1.1 = RXD, P1.2=TXD
    P1DIR |= RXLED + TXLED;
    P1OUT &= 0x00;
    UCA0CTL1 |= UCSSEL_2; // SMCLK
    UCA0BR0 = 0x08; // 1MHz 115200
    UCA0BR1 = 0x00; // 1MHz 115200
    UCA0MCTL = UCBRS2 + UCBRS0; // Modulation UCBRSx = 5
    UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**

    while(1)
    {
    if(URXIFG0==1)
    {
    UCA0TXBUF = UCA0RXBUF;

    }


    P1OUT^=BIT0;
    }

    }

  • Hi Surya,

    You should use those code in while(1) :

          if(IFG2&UCA0RXIFG)
          {
              UCA0TXBUF = UCA0RXBUF;
          }

    Best Regards

    Johnson

**Attention** This is a public forum