This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430I2041: Circuit design checked

Part Number: MSP430I2041

Dear Support,

Can you please checked our controller design of analog section, uart section, oscillator section, Vref pin used, programming pins of controller.

MSP430I2041TPW.pdf

  • Hello,

    Here are my observations based on the attached PDF:

    • The capacitor on VCORE is correct (470nF)
    • The resistor on ROSC is correct (20KOhms)
    • The capacitor on VREF is correct (100nF)
    • The programming pins look correct based on the MSP430 Hardware Tools User's Guide
    • VCC filtering caps look good
    • The I2C pull-up resistor values are based on the capacitance on the node. 4.7KOhm should suffice
    • Everything else looks accurately labelled

    Best regards,

    Matt

**Attention** This is a public forum