Part Number: MSP-EXP432P401R
Other Parts Discussed in Thread: MSP430FR5989
Hello everyone!
I am looking for a software example(or some general explaining) that helps with the flash memory.
Previously I was using MCUs with FRAM only(msp430fr5989).
I would like to achieve persistent variables but so far I wasnt successful.
I understand that the logic is read-modify-write.
My questions:
How can I create a persistent variable(fore. uchar)?
Do I have to follow the read-modify-write algorythm? or can I do modify-write only?(thinking about something like var++, where var is persistent),
How do I use the variables that I store in flash?
When I am using them are they moved to the ram?
As I understand, I should not write my variables new value everytime they change, right?
I think this beacuse of the limited amount of read/write on flash memory. Correct me if I am wrong.
I looked at the flash_program_memory software example on dev.ti.com, but i couldnt figure it out.
Also I checked slaa704 and slau356i but i couldnt exactly figure it out.
Bálint