Part Number: MSP430FR5969
Other Parts Discussed in Thread: ENERGIA
Tool/software: Code Composer Studio
Hello there,
I have been trying to use a MSP430FR5969 Launchpad evaluation kit to start a serial communication with a SARA-R4 Cellphone modem.
Basically that modem just works sending AT commands through serial communication, so, i decided to start with the basics using the library example
include <SoftwareSerial.h>
SoftwareSerial mySerial(P1_4, P1_3);// RX, TX
void setup(){ // Open serial communications and wait for port to open:
Serial.begin(9600);
Serial.println("Goodnight moon!"); // set the data rate for the SoftwareSerial port
mySerial.begin(9600);
mySerial.println("Hello, world?");
}
void loop(){ // run over and over
if(mySerial.available())
Serial.write(mySerial.read());
if (Serial.available())
mySerial.write(Serial.read());
}
Unfortunately an error jumps everytime i try to compile the code.
C:\Users\dom\Desktop\energia-1.8.7E21\hardware\energia\msp430\libraries\SoftwareSerial\SoftwareSerial.cpp:80:2: error: #error This version of SoftwareSerial supports only 16MHz processors C:\Users\dom\Desktop\energia-1.8.7E21\hardware\energia\msp430\libraries\SoftwareSerial\SoftwareSerial.cpp: In member function 'void SoftwareSerial::begin(long int)': C:\Users\dom\Desktop\energia-1.8.7E21\hardware\energia\msp430\libraries\SoftwareSerial\SoftwareSerial.cpp:250:31: error: 'table' was not declared in this scope C:\Users\dom\Desktop\energia-1.8.7E21\hardware\energia\msp430\libraries\SoftwareSerial\SoftwareSerial.cpp: In member function 'virtual size_t SoftwareSerial::write(uint8_t)': C:\Users\dom\Desktop\energia-1.8.7E21\hardware\energia\msp430\libraries\SoftwareSerial\SoftwareSerial.cpp:318:26: error: 'XMIT_START_ADJUSTMENT' was not declared in this scope exit status 1 Error compilando para la tarjeta MSP-EXP430FR5969LP.
So i decided to debug the library looking for those lines and trying to solve the errors that way, but after a few days i still can not get rid of that compiling error.
Does anyone has an idea about what is happening and how can i solve it?
Regards