This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5522 UART BSL

Other Parts Discussed in Thread: MSP430F5522, MSP430F5510

Hi,

I'm using the MSP430F5522 in a new product design. On page 21 of the datasheet for the MSP430F552X, there is a statement about the UART BSL:

A UART BSL is also available that can be programmed by the user into the BSL memory by replacing the pre-programmed, factory supplied, USB BSL.

In SLAU319A, "MSP430 Programming Via the Bootstrap Loader" there is the following statement in section 5.1 for the MSP430F552x family:

BSL in device is RAM write only. Full BSL must first be loaded into device RAM and started to perform flash write.

I've looked and I can't find the "full BSL" for the UART BSL communications. I'm not using USB with this chip, so that's not an option. I'm looking to download new firmwareinto this chip from another processor (not a PC).

Thanks,

Scott

**Attention** This is a public forum