The MSP430L092 Development Guide SLAA472A contains the following description of the Copy application to external SPI memory after program load option:
I.e. the same paragraph is repeated twice.
I think the text should be:
For download and debug from RAM, uncheck the Copy application to external SPI memory after program load checkbox as shown in Figure 18.For download and debug from EEPROM, check the Copy application to external SPI memory after program load checkbox as shown in Figure 18.