Other Parts Discussed in Thread: MSP430F5419, CC430F6137, CC1101, MSP430F5438A
I had ordered the CC430 Wireless Development Kit. It has MSP430F5xx core and supports all CC430F613x and CC430F612x flash parts.
What is meant by flash parts? How are those different from the core? MSP430 is a microcontroller, right? So it must have the flash in itself? (sorry, I am a beginner.)
I run Windows 7 Ultimate 64-bit edition.
I also downloaded and installed Code Composer Studio v4 for MSP430. This is my first time using CCS and so I followed the instructions on the welcome screen. The "Flashing the LED" example worked flawlessly. However, then I tried to import an existing project from:
<Installation root>\Texas Instruments\ccsv4\msp430\examples\example projects\msp430x5xx C Example
It gave an error with configuration file not matching the hardware. So, I had to replace the configuration file initially. It was MSP430F5419.ccxml (which gave an error). So I copied CC430F6137.ccxml from flashing the LED project. Is this alright/allowed?? Can I do this??
Then, when I click, Target ---> Debug Active Project, I come up with the following error:
MSP430: Trouble Writing Memory Block at 0x5c00 on Page 0 of Length 0x22: Could not write device memory
Cannot write to target
How can I solve this??
I tried to access check the address in the memory map documentation (user guide slau259b, pg. 37). The memory locations are from 00000h to FFFFFh (5 digits). However, the error is at 0x5c00 ('5c00' is four digits). So, is 0x5c00 = 05c00h?? (That would be at the starting locations of the memory then).
Also, when I go to View--->Memory, it opens a new window on the right. However, everything is grayed out. I cannot enter the memory location. I wanted to check if the memory at 0x5c00 can be written to or not. How can I check memory locations?
Sorry about too many questions. I am eager to learn more and at the same time in need of guidance.
Thank you very much, everyone, for the help and the time. I appreciate it. :)